Technical FAQs

Ask a Question

Do you offer a key operated 2510 manual switch in a NEMA 4 enclosure?

Issue:
Do you offer a key operated 2510 manual switch in a NEMA 4 enclosure?

Product Line:
2510 Manual Switches

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
There is no option for a key operated class 2510 manual switch in a NEMA 4, OR NEMA 7 & 9 enclosure. The only option is to use a general purpose enclosure.
 
Was this helpful?
What can we do to improve the information ?