Technical FAQs

Ask a Question

What is the Inrush and Sealed current of the AC coils for the LC1D115, and LC1D150?

Issue:
What is the Inrush and Sealed current of the AC coils for the LC1D115, and LC1D150?

Product Line:
TeSys D-Line Contactors

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:
For all 50/60 Hz AC coil voltages, the Inrush current is 350VA, and the Sealed current is 18VA.
Was this helpful?
What can we do to improve the information ?