Technical FAQs

Ask a Question

What are the dimensions of the 9991SCW2 NEMA 4 oversized enclosure?

Issue:
What are the dimensions of the 9991SCW2 NEMA 4 oversized enclosure?

Product Line:
9991 NEMA 4 Enclosures

Environment:
Dimensional Information 

Cause:
Product Features 

Resolution:
Width = 12.63"/321mm
Height = 7.81"/198mm
Depth = 14.69"/373mm
Was this helpful?
What can we do to improve the information ?