Technical FAQs

Ask a Question

What are the dimensions of the 9991SDA11 NEMA 12/3R enclosure?

Issue:
What are the dimensions of the 9991SDA11 enclosure.

Product Line:
9991 NEMA 12/3R Enclosures

Environment:
Product features 

Cause:
Dimensional Information 

Resolution:
Width = 8.13"/206mm
Height = 9.28"/236mm
Depth = 16.00"/406mm
Was this helpful?
What can we do to improve the information ?