Technical FAQs

Ask a Question

What is the catalog number for the vertically mounted main breaker that is included with the HCN18652MN interior assembly ?

ISSUE
What is the catalog number for the vertically mounted main breaker that is included with the HCN18652MN interior assembly ?

PRODUCT LINE
I-line panelboard sold and supported in the USA. 

ENVIRONMENT
Identification 

CAUSE
Replacement .

KEY WORDS
Iline I line panelboard panel board main breaker circuit powerpact power pact interior assembly HCN18652MN

RESOLUTION
JDL36225 
Was this helpful?
What can we do to improve the information ?