Technical FAQs

Ask a Question

How do I unlock the ATV312 drive using the universal pass code?

Issue:
Unlock ATV312

Product Line:
ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
The universal unlocking code for the ATV312 drive is 6969.  The instructions for unlocking the ATV312 is as follows:
1. When the drive says "RdY" press enter on the dial
2. Rotate the dial to menu "SUP" and press enter.
3. Rotate the dial to "Cod" and press enter (If a pass code has been enabled the display should show "On")
4. Rotate the dial (you should see the numbers increase) until you reach "6969" then press enter (the display should say "off").
5. Press the "ESC" button two times back to "SUP".  You should be able to access all menus.
 
Was this helpful?
What can we do to improve the information ?