Technical FAQs

Ask a Question

Hand Off Auto switch for 2510FG

Issue:
What is the part number for a 2510F*72 or 2510F*71 HOA replacement?

Product Line:
2510 Maual Starters - GIC Product
2510FG71, 2510FF71, 2510FS71 with or without P form
2510FG72, 2510FF72, 2510FS72 with or without P form

Environment:
US Product

Cause:
This switch may need to be replaced and the part number is not specified in the Digest

Resolution:
Use part number 31057-549-50.  This includes the switch, handle and legend.
 
Was this helpful?
What can we do to improve the information ?