Technical FAQs

Ask a Question

What are the repair parts for a J250R, Series A01 circuit breaker enclosure?

Issue:
Repair parts

Product Line:
Circuit Breaker Enclosure

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 40515-843-50 (NOTE: The cover does not have the nameplate applied)
Cover Mounting Screws - 40205-130-02K
Circuit Breaker Cover - BCV (This is the smaller plastic cover that is attached to the larger metal cover)
Top Endwall Closing Cap - ACPL



CTA-ID : 5937
Was this helpful?
What can we do to improve the information ?