Technical FAQs

Ask a Question

What is the continuous current rating of a 2510 type F starter?

Issue: What is the continuous current rating of a 2510 type F starter?

.
Product Line:  NEMA Class 2510 Type F, 2510FO, 2510FG, 2510FF, 2510FS, 2510FW, 2510FR


Environment: Unique to the 2510 Type F manual motor starters


Cause: Continuous Current Rating

Resolution: Continuous current rating is 16A

Was this helpful?
What can we do to improve the information ?