Technical FAQs

Ask a Question

What is the neutral lug data for a NF466L4C ?

Issue:
Terminal data for neutral

Product Line:
Panelboards

Environment:
NF

Cause:
Installation

Resolution:
The main neutral lugs are for 2- 1/0 -300kcmil or 1- 1/0-750kcmil cable . The branch lugs are for 8- #14-2/0 and 34-#14-#6 AL or CU .
 

Was this helpful?
What can we do to improve the information ?