Technical FAQs

Ask a Question

When the Conext SW is in passthrough, what is the units output voltage?

Customers want to confirm when the Conext SW is in passthrough, what is the units output voltage when using a 120v (Mono Phase) AC source? 

When the unit is in passthrough using a 120V source, the output will be 120V/240V.

 
Was this helpful?
What can we do to improve the information ?