Technical FAQs

Ask a Question

What is the part number for the IMC card for the ATV61 or ATV71 drive?

Issue:
What is the part number for the IMC card for the ATV61 or ATV71 drive?

Product Line:
ATV61 and ATV71 Drives
 

Environment:
All serial numbers for ATV61/71 Drives

Cause:
N/A

Resolution:
VW3A3521
VW3A3521S0 was an old part number which is now obsolete

Was this helpful?
What can we do to improve the information ?