Technical FAQs

Ask a Question

Will Push-to-test operators increase the enclosure size of a combination starter.

Issue:
Will Push-to-test operators increase the enclosure size of a combination starter.

Product Line:
NEMA 8538 Combination Starters - GIC Product

Environment:
US Product

Cause:
Enclosure size can be an important design consideration

Resolution:
Yes, the push-to-test operator option will cause the enclosure to default to a larger size.
Was this helpful?
What can we do to improve the information ?