Technical FAQs

Ask a Question

What is the default enclosure size for an R44 relay option on a combination starter?

Issue:
What is the default enclosure size for an R44 relay option on a combination starter?

Product Line:
NEMA Combination Starters - GIC Product

Environment:
US Product

Cause:
Enclosure size is an important design criteria

Resolution:
The R44 relay option is for a phase failure relay and wll cause the enclosure size to default to an oversize option.  This cannot be modified.
Was this helpful?
What can we do to improve the information ?