Technical FAQs

Ask a Question

What is the insulation class of the coils fitted within the NEW TESYS 'D' range D09 to D150

 

Issue:
What is the insulation class of the coils fitted within the NEW TESYS 'D' range D09 to D150.

Product Line: 
TESYS D, LC1D09 - LC1D150

Environment:
Unique to the LC1D product line


Cause:
Insulation class for product knowledge

Resolution
The class of the wires of the contactor coils is H
The rated insulation voltage is : 690V up to LC1D32
( remark : today for contactors from LC1D40 to LC1D150 ) there is not electrical characteristic changes acording to the D2 line

Was this helpful?
What can we do to improve the information ?