Technical FAQs

Ask a Question

Can the ATV312 (Altivar 312) drives be used with single phase input power to run 3 phase motors?

Issue:
Application with single phase line voltage.

Product Line:
ATV312

Environment:
All

Cause:
Single phase line voltage only

Resolution:
YES, with certain limits.

Download the "Annex for ATV312 Quick Start Guide" for details on SSCR, branch circuit protection and approved single phase input sizing information.
Note the requirement for Line Reactors on many of the part numbers.

http://www.schneider-electric.us/en/download/document/S1B16328/

When using 3 phase drives on single phase input, you must change the IPL (Input Phase Loss) parameter from YES to NO.  This parameter is found in the FLt (Fault) menu.
Was this helpful?
What can we do to improve the information ?