Technical FAQs

Ask a Question

What comes in the box when you order the B thermal units (heaters)?

Issue:
What comes in the box when you order the B thermal units (heaters)?

Product Line:
8536 Type S Starters

Environment:
US Product Lines

Cause:
I need to know if they come with screws

Resolution:
This will come with only the thermal unit itself; the B thermal units do not come with screws. You will need to use the screws installed on the overload of your starter.
Was this helpful?
What can we do to improve the information ?