Technical FAQs

Ask a Question

Micrologic A, P, H Trip Unit Dials Compared Side by Side - M, P, R, NT, NW Circuit breakers

Issue:
Comparing Trip Units
Compare Trip Units

Product Line:
Trip Units used in Powerpact M, P, R, and Masterpact NT and NW Breakers
Basic Trip Units ET1.0 and ET1.0I
Micrologic Standard Trip Units 2.0, 3.0, 5.0
Micrologic Ammeter Trip Units 2.0A, 3.0A, 5.0A, 6.0A
Micrologic Power Trip Units 5.0P, 6.0P
Micrologic Harmonic Trip Units 5.0H, 6.0H

Resolution:
The attached file shows
-Details of each trip unit
-Side-by-side comparison of the dials
-Values of ground fault Ig letters A - J
-Values of rating plugs A-H
-Explanation of Ir, tr, Isd, tg, Ii, Ig, tg, In
Was this helpful?
What can we do to improve the information ?