Technical FAQs

Ask a Question

Magentic Safety Interlock in 120V

Issue:
Are Magnetic Safety Interlock switches available in 120V?

Product Line:
Preventa Safety Switches - GIC Product

Environment:
US Product

Cause:
Misapplication of switch causes this confusion

Resolution:
These switches should only be powered by a safety relay.  The contacts are designed to only accept a very low amperage 24V signal.  These switches should not be used in general circuits with a direct supply of power.
 
Was this helpful?
What can we do to improve the information ?