Technical FAQs

Ask a Question

How many rack in/out operations is the Masterpact cradle rated for?

Product Line:
Masterpact NW

Resolution:
The rack in/rack out durability requirements of IEC 60947-2  and IEC61439 are 200 operations.
We have tested it to 500 operations.
 
Was this helpful?
What can we do to improve the information ?