Technical FAQs

Ask a Question

Can an 8536SCO1 be converted to a 8536SCO2

Issue:
Can an 8536SCO1 be converted to a 8536SCO2?

Product Line:
8536S NEMA Starters - GIC Product

Environment:
US Product

Cause:
One of these starters is a size 1, and the other is a size 1P.

Resolution:
The 8536SCO1 cannot be converted to an 8536SCO2.  The 8536SCO2 has been specifically tested to conform to NEMA size 1P.  The 8536SCO1 has not been tested for this standard and therefore will not conform to it rgardless of modification.
 
Was this helpful?
What can we do to improve the information ?