Technical FAQs

Ask a Question

Can more than 1 9999SN1 kit be installed into an enclosed 8903 lighting contactor?

Issue:
Needs to land additional neutrals, more than allowed by 9999SN1.

Product Line:
9999SN1 kit

Environment:
Products sold and used in the United States
 
Resolution:
There is not enough space in the enclosure. If this is required of application, use open type and third party enclosure large enough to accomodate the additional modules.
 

Was this helpful?
What can we do to improve the information ?