Technical FAQs

Ask a Question

Is an electrical interlock available for the DTU224NRB, DTU324NRB or DTU324N?

Issue:
Product features

Product Line:
Double throw safety switch

Environment:
Applies only to catalog numbers listed in question

Cause:
Product feature availability

Resolution:
Yes, but only factory installed. Add suffix EI to have 2NO/2NC aux contacts in both operating positions. Not UL Listed.

Was this helpful?
What can we do to improve the information ?