Technical FAQs

Ask a Question

Customer is trying to functionality test on a Conext Battery Monitor

Customers who are installing a new Conext Battery Monitor and they want to test the functionality of the unit for RMA. 

*Example is for a 48V battery bank (for a 24V battery bank, check for 24V) 

1 . Test from point G (V-) to H (V+) - Voltage should be 48V
2. Test from point E (Vm-) to F (Vm)  - Voltage should be 48V
3. Check the two inline fuses 
4. With a small screw check the input wire connections 

If voltage is present to the inverter (48V) and the fuses are good and the wires are properly seated, RMA the unit.
Was this helpful?
What can we do to improve the information ?