Technical FAQs

Ask a Question

Can ATV31 file be uploaded and then downloaded to ATV312 using SoMove software?

Issue:
Can ATV31 file be uploaded and then downloaded to ATV312 using SoMove software?

Product line:
Altivar ATV31, ATV312

Environment:
All models, all serial numbers

Cause:
Need to connect to Blue Hose

Resolution:
It is not possible to transfer a configuration from ATV31 to ATV312 with SoMove software.  you will have to use the multiloader or the old ATV31 keypad to copy an 31 file into the ATV312 drive if you configure the ArE parameter to 31A or 31 E.
The better solution is to generate the configuration file in Off-line Project for ATV312 then upload to Drives.
Was this helpful?
What can we do to improve the information ?