Technical FAQs

Ask a Question

ATV12 Jog not working with Modbus as reference.

Issue:
ATV12 Jog not working with Modbus as reference.

Product Line:
Altivar 12

Environment:
All 

Cause:
ATV12 Jog not working with Modbus as reference.

Resolution:
Modbus reference, Terminal control.  FLO needs to be assigned to same logic input as JOG. Jog is a fixed speed of 5Hz.
Was this helpful?
What can we do to improve the information ?