Technical FAQs

Ask a Question

What nameplate options are available for panelboards?

Product Line:
Panelboards

Environment:
Applies to NQ, NF, I-Line Combo, I-Line and QMB panelboards.

Resolution:
  1. Nameplates are offered in three sizes and can have multiple line per nameplate (see photo below for relative size comparison and EXCEL attachment for additional details).
  2. Nameplates are offered in eight color combinations (see photo below for approximate color reference and EXCEL attachment for additional details).
  3. Nameplates are offered with an adhesive backing but optional screws are also available.
  4. Nameplates are installed by the customer.
  5. Special nameplates are not available. The customer will need to get nameplates from an outside source for sizes and colors not listed in the attachment.
  6. Local trophy shops are a good source for special nameplates.


Was this helpful?
What can we do to improve the information ?