Technical FAQs

Ask a Question

What would be the replacement to the older ATV31 S-Flex drive?

Issue:
What would be the replacement to the older ATV31 S-Flex drive?

Product Line:
ATV31 S-Flex

Environment: 

All

Answer To Customer: 
If the application is low torque such as fan or pump then an ATV212 S-Flex would be a good replacement.
If the application is moderate or heavy torque, then please contact your local Product Application Engineer (PAE) or local distributor for enclosed drive selection.
Was this helpful?
What can we do to improve the information ?