Technical FAQs

Ask a Question

IEC vs ULApproved EVlink Charging Stations

Issue:
Inquiry about a European EVlink Charging Station.  

Product Line:
Electric Vehicle Service Equipment (EVSE)

Cause:
Due to different electrical standards, the EV charging stations offered in some geographic regions are different than others.   A UL/CSA/ANCE Listed series of EVSE's are distributed in North America.  These stations may also be used in South America.  Schneider Electric also offers IEC approved EVlink charging stations for use in Europe, Africa, Asia, and Australia.

Resolution:
The IEC approved charging stations in the 04.2014 catalog are listed below.
These items are not distributed or supported in North America.  

NCA19130, NCA19330, NCA11130, NCA11230, NCA11100, NCA19310, NCA00100, EVH1S3P03, EVH1S7P03, EVH1S3P0A,  EVH1S7P0A, EVH1S2P0C, EVH1S7P0C, 
EVF1S7P02 EVF1S7P02R EVF1S7P03 EVF1S7P03R EVF1S7P22 EVF1S7P22R EVF1S7P33 EVF1S7P33R EVF1S22P02 EVF1S22P02R EVF1S22P03 EVF1S22P03R EVF1S22P22 EVF1S22P22R EVF1S22P33 EVF1S22P33R  
EVW1S7P02 EVW1S7P02R EVW1S7P03 EVW1S7P03R EVW1S7P22 EVW1S7P22R EVW1S7P33 EVW1S7P33R EVW1S22P02  EVW1S22P02R EVW1S22P03 EVW1S22P03R EVW1S22P22 EVW1S22P22R EVW1S22P33
EVW1S22P33R  EVP1PH EVP1WPSC


UL approved charging stations for USA and Canada include the following part numbers:

EV230WS EV230WSR EV230PSR EV230PDR EV230WSRR EV230PSRR EV230PDRR EV230PDRACG EV230PDRACGC EV230PDRACNG EV230PSRACG EV230PSRACGC EV230PSRACNG EV230WDRACG EV230WDRACGC EV230WDRACNG


 
Was this helpful?
What can we do to improve the information ?