Technical FAQs

Ask a Question

Is an enclosure available for the LA36350 circuit breaker?

Issue:
Selection

Product Line:
Circuit Breaker Enclosure

Environment:
Selection

Cause:
Selection

Resolution:
The LA36350 is an I-Line breaker suitable only for use in applicable I-Line panel boards. There is no individually mounted enclosure for any I-Line circuit breaker.
Was this helpful?
What can we do to improve the information ?