Technical FAQs

Ask a Question

How do I size my XW+NA inverter?

Inverter sizing must be calculated for the maximum load possible in a backup scenario so the inverter is not overloaded. 
Even though the XW+NA can pass thru 60A, the designer must consider maximum continuous output rating to properly size inverter system.
Was this helpful?
What can we do to improve the information ?