Technical FAQs

Ask a Question

What mechanical interlock is used to link an LC1F400 with an LC1F265 or LC1F330?

Issue:
What mechanical interlock is used to link an LC1F400 with an LC1F265 or LC1F330?

Product Line:
TeSys F-Line Contactors

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:
Use part number LA9FJ4H.
This is for vertical mounting only. The LC1F265/LC1F330 MUST be mounted below the LC1F400.
Was this helpful?
What can we do to improve the information ?