Technical FAQs

Ask a Question

Can I see the status of the analog / logic inputs of the ATV61/71 series drives on the keypad?

Issue:
Can I see the status of the analog / logic inputs of the ATV61/71 series drives on the keypad?

Product Line:
Altivar 61 and Altivar 71 series drives equipped with VW3A1101 keypad.

Environment:
All models, All serial numbers, VW3A1101 equipped

Cause:
Customer needs to display this information for troubleshooting / installation purposes.

Resolution:
From the main menu, select Drive menu (menu 1) then Monitoring menu (Menu 1.2)   Under Monitoring menu, select I/O map.   From here, to display the incoming voltage/current to the analog inputs, select Analog Inputs Image.   To display the status of the logic inputs, select Logic Input Map.
Was this helpful?
What can we do to improve the information ?