Technical FAQs

Ask a Question

Does XW+NA Aux provide output voltage or is it a dry relay contact?

XW+NA Aux port provides a 12VDC@250mA signal when active. This can be used to drive an external dry relay contact provided 
the coil is 12VDC at no more than 250mA.
Was this helpful?
What can we do to improve the information ?