Technical FAQs

Ask a Question

Why is my Conext SW Inverter/Charger faulting with F2 (AC output Over voltage)?

Conext SW Inverter/Charger is faulting with F2

Problem: Conext SW is faulting with F2(AC Output Over Voltage)
Solution:  Check the firmware and make sure it is 3.0.
The trip limits on the 3.0 were increased so it is most likely the CSW has older firmware.
Was this helpful?
What can we do to improve the information ?