Technical FAQs

Ask a Question

What is the W suffix in the part number LGA34250WU31X

Issue:
What does the W represent in the part number for the LGA breaker?

Product Line:
LGA Molded Case Circuit Breaker

Environment:
LG, LD, LJ and LL Electronic Trip Mission Critical Circuit Breakers

Cause:
What does the W represent?

Resolution:
The W represents a Mission Critical breaker and it is used with Powerpact J and L frame. The voltage code on these breakers is 4 (480Vac) instead of 6 (600Vac)


 
Was this helpful?
What can we do to improve the information ?