Technical FAQs

Ask a Question

Why is my Trace SW reporting the wrong battery voltage in METERS?

Sometimes the battery temp sensor (BTS) can go bad, resulting in an erroneous voltage being reported, leading to erratic behavior and Hi/Lo battery errors.
If reading of the Temp Comp volts and Battery Actual volts is > 2V difference, the BTS is likely bad.

Solution : Replace BTS 
Manuf Pt # 130-0004-01-01
http://www.civicsolar.com/product/xantrex-bts-35-battery-temperature-sensor-w-35ft-cable
Was this helpful?
What can we do to improve the information ?