Technical FAQs

Ask a Question

Does XW+NA interact with lithium-ion battery management system (BMS)?

No, the XW+NA does not interact directly with lithium-ion BMS systems.
The Combox has modbus capability, as do some BMS systems, so it may be possible
to have the two systems interact in some way. The XW+NA does provide a charge algorithm
that may be applied to a lithium-ion battery bank, however the battery manufacturer has the final
say on what charge voltage and current their batteries should be charged at. Battery management systems
for lithium batteries are usually stand-alone systems that interrupt the battery circuit if one or more batteries reach
a certain high temperature, or control temperature by balancing of cells. 
 
Was this helpful?
What can we do to improve the information ?