Technical FAQs

Ask a Question

Can the ATV312 communicate with Modbus and Canopen at the same time?

Issue:
Can the ATV312 communicate with Modbus and Canopen at the same time?

Product Line:
ATV31 ATV312

Environment:
All

Cause:
Application requirement

Resolution:
No, the drive can only have one communication protocol at a time.
 
Was this helpful?
What can we do to improve the information ?