Technical FAQs

Ask a Question

Does NFN6CU come with the bonding strap?

Does NFN6CU come with the bonding strap?

Product Line:

UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Service entrance applications require that the neutral be bonded to ground.  This is accomplished with the installation of neutral bonding hardware.

No NFN6CU does not include the bonding strap. The bonding strap is ordered using part number 80113-675-51.

Was this helpful?
What can we do to improve the information ?