Technical FAQs

Ask a Question

Can I use a modified sine wave on an ATS01 Soft Start

Issue:
Modified sine wave

Product Line:
ATS01 Soft Start

Environment:
All models and serial numbers

Cause:
None

Resolution:
It is not recommended to use a modified sine wave on an ATS01.  A modified sine wave has abrupt changes.  The SCR's in the ATS01 may not see a zero cross over which can affect their conduction.
 
Was this helpful?
What can we do to improve the information ?