Technical FAQs

Ask a Question

What is the pin out for ATV66 keypad cable?

Issue:
What is the pin out for ATV66 keypad cable?

Product Line:
ATV66, Altivar 66

Environment:
All

Cause:
To connect a keypad remotely

Resolution:
The pin outs are as follows:
Signal: DA, 0 VDC, DB, +VDC.
ATV66 pin out respective:
Pin 3  - DA
Pin 4  - 0 VDC
Pin 7  - DB
Pin 9 - +VDC
 
Was this helpful?
What can we do to improve the information ?