Technical FAQs

Ask a Question

What is the Door only dimension for a NC68VS trim?

 Issue:
What is the Door only dimension for a NC68VS trim?

Product Line:
NQ/NF Panelboards

Environment:
Space restriction

Cause:
Clearance measurement clarification

Resolution:
For the NC68VS trim the ​Door opening is 45.24"H x 12.93"W. Door/cover only dimension is 45.14"H x 12.83"W
  
Was this helpful?
What can we do to improve the information ?