Technical FAQs

Ask a Question

What is a MH50B24 and can anything be used in its place ?

Issue:
Special enclosure

Product Line:
Panelboards

Environment:
NQ , NF

Cause:
B24 suffix

Resolution:

This is an indoor box with a 24"h bottom extension ....all one piece. A MH50 with a WW24 ( which is a 24"h add-on wireway) would be fairly comparable
 
 
 
 
Was this helpful?
What can we do to improve the information ?