Technical FAQs

Ask a Question

Where can I find a listing of GT 1-PH fuse sizes?

  • GT2.5
    15A, 250Vac SLOW-BLOW 3AB CERAMIC Fuse
    BUSSMANN MDA-15 or equivalent
    1.25" x 0.25"
  • GT2.8 / TX2800
    15A, 250Vac SLOW-BLOW 3AB CERAMIC Fuse
    BUSSMANN MDA-15 or equivalent
    1.25" x 0.25"
  • GT3.0
    20A, 250Vac SLOW-BLOW 3AB CERAMIC Fuse
    LITTELFUSE 326-020 or equivalent
    1.25" x 0.25"
  • GT3.3 / TX3300
    20A, 250Vac SLOW-BLOW 3AB CERAMIC Fuse
    LITTELFUSE 326-020 or equivalent
    1.25" x 0.25"
     
  • GT3.8 / TX3800
    25A, 250Vac SLOW-BLOW 5AB CERAMIC fuse
    LITTELFUSE FLM 25 or equivalent
    1.50" x 0.406"
  • GT4.0
    25A, 250Vac SLOW-BLOW 5AB CERAMIC fuse
    LITTELFUSE FLM 25 or equivalent
    1.50" x 0.406"
  • GT5.0 / TX5000
    30A, 250Vac SLOW-BLOW 5AB CERAMIC fuse
    LITTELFUSE FLM 30 or equivalent
    1.50" x 0.406"
     
  • ALL MODELS :  DC Ground Fault Fuse600 Volt, 1 Amp ground fault fuse (replace with Littelfuse KLKD 1 or equivalent)
Was this helpful?
What can we do to improve the information ?