Technical FAQs

Ask a Question

What is the mechanical interlock for LC1F330/3304 and LC1F185/265/1854/2654 contactors?

I need an interlock for (2) LC1F contactors with different amperage ratings.

Product Line:
TeSys F-Line Contactors

All Product Lines

Can not find it in the Digest

To interlock the LC1F330 (3 or 4 pole) and the LC1F185 OR LC1F265 (3 or 4 pole) use part number LA9FH4G*
This is for vertical mounting only.

*lower contactor must have equal or lower current rating
Was this helpful?
What can we do to improve the information ?