Technical FAQs

Ask a Question

What is the mechanical interlock for the LC1F500/5004 and LC1F265/265/330/3304 contactors?

Issue:
I need a mechanical interlock for the LC1F500 (3 or 4 pole), and the LC1F265 (3 or 4 pole) OR the LC1F330 (3 or 4 pole).

Product Line:
TeSys F-Line Contactors

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:
To mechanically interlock the LC1F500 (3 or 4 pole) with the LC1F265 (3 or 4 pole) OR the LC1F330 (3 or 4 pole), use part number LA9FK4H.

This is for vertical mounting ONLY, and the contactor with the lower amperage rating must be the bottom contactor.
Was this helpful?
What can we do to improve the information ?