Technical FAQs

Ask a Question

What is the mechanical interlock for the LC1F630/6304 and LC1F500/5004 contactors?

I need a mechanical interlock for the LC1F630 (3 or 4 pole), and the LC1F500 (3 or 4 pole).

Product Line:
TeSys F-Line Contactors

All Product Lines

Can not find it in the Digest

To mechanically interlock the LC1F630 (3 or 4 pole) with the LC1F500 (3 or 4 pole), use part number LA9FL4K.

This is for vertical mounting ONLY, and the contactor with the lower amperage rating must be the bottom contactor.
Was this helpful?
What can we do to improve the information ?