Technical FAQs

Ask a Question

Can I upgrade an E-Flex to a larger drive size by changing the ATV61 drive?

Issue:
Can I upgrade an E-Flex to a larger drive size by changing the ATV61 drive?

Product:
E-Flex

Environment:
All

Cause:
Can I change drive from an 25hp to a 30hp, for a 30hp rating?

Resolution:
No, not recommended. The E-Flex is designed for the horsepower rating it was order for.
Other E-Flex components and certifications must be considered. This would include wire size, breaker size, contactors (if bypass).
This could void the warranty and the UL listing.



 
Was this helpful?
What can we do to improve the information ?