Technical FAQs

Ask a Question

What are the repair parts for a H326DS and H326NDS Series E5 (or E05) Heavy Duty Safety Switches?

Issue:
Current design repair parts

Product Line:
Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The parts listed here are the only field replaceable parts.

Line base assembly - 4055218552 (3-required and arc suppressor assembly included)
Load base assembly - 4055218750SEL (3-required)
Arc suppressor assembly - 4051204501 (3-required)
Lug assembly - 4405044601 (2 required per base assembly)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Operating handle assembly - 4051219151
Operating handle mounting screws and washers - 2140122242(screw - 2 required) and 2370100220(washer - 2 required) 

Handle knob kit - 4401142750 (the black & red knob at the end of the handle)
Neutral assembly - H600SN (Field installable neutral and comes standard with Neutral bonding strap)

Neutral bonding strap - 4028300750 (used on the H326NDS)
Door Thumb Screws and retainers -  S1A99898(Thumb Screw - 2 required) and 4405043301(Retainer - 2 required)
Cross bar insulator - 4055217801 (1-required and is red in color and approximately 8.85" long x 1.5" high)
Cross bar insulators - 4055217701 (2-required and is red in color and approximately 4.19" long x 2.5" high)
Dust shield - 4055215701 (1 required, usually red in color and is approximately 16.10" long x 1.16" wide)



 
Was this helpful?
What can we do to improve the information ?